Browse FAQs

What can cause an INFD or internal error 13 on the ATV630 and ATV930 Process Drives?

Published date: 09 December 2019

Issue:
What is the INFD fault on the ATV630 and ATV930 drives?

Product Line:
ATV630 ATV930

Environment:
All model numbers, all serial numbers

Cause:
One or more Brick are not in operation
Current transformer of the brick damaged

Resolution:

  • Check the high speed link cables (GG45) on the Power board (CMP6) and the Inverter Bricks (CMI1).  This happens if not all pins of the connector have a good connection.
  • Measurement of the U/V/W phase currents of each brick on the paralleling choke to identify the brick with less output current.
  • Manual IGBT test of each Brick with a multimeter (open Motor choke connections)
  • Check the Inverter board and the CMI1 board (the communication board on the Inverter board) for visible damages.
  • Run the motor for a certain time (if possible) and check the thermal state of each brick.  The one with a lower temperature does not switch on the IGBTs and has to be replaced.
  1.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.