Browse FAQs

What is the Environmental Rating of the HMIPCCU27?

Published date: 26 July 2019

Issue
How do I find the is the Environmental Rating of the HMIPCCU27 if it is comprised of two parts?

Product Line
Magelis Modular Box PC HMI

Environment
Physical HMI

Resolution
Since the HMIPCC is comprised of the Front Screen and Back CPU unit, the Environmental Rating is of the screen when mounted flush with the gasket.
The Rating for the screen is IP66 and NEMA 4X.
 
The HMIPCCU27 will essentially be comprised of one of these Modular Box Universal modules (depending on desired configuration) plus a specific touchscreen:

Modular Box Universal:
https://www.se.com/us/en/product-range/61054-magelis-industrial-pc/?N=2360390577+567237335&_requestid=189658&Nrpp=20#tabs
There's essentially two sizes (2 slot and 4 slot), and you can click on each one to get the CAD files and Mounting dimensions on their datasheet pages.
 
15" touchscreen - HMIDM7421:
https://www.se.com/us/en/product/HMIDM7421/display-pc-4%3A3-15%22-single-touch-for-hmibm/?range=61054-magelis-industrial-pc&node=684640674-box,-rack-&-display
 
In the Characteristics page of the HMIDM7421, if you scroll down, you'll see that the Environmental Rating for this 15" touchscreen is:
IP66 and NEMA 4X

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.