Browse FAQs

Preventa XCS - How to order the XCSZC7912 part number

Published date: 29 July 2019

Find attached the picture of both part XCSZC1 magnet and XCSZC7912 detector having a 2m cable length, which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMC7912. Switch has a LED. Same situation for the XCSZC79110 part number (10m cable length) : to be order under complete reference XCSDMC79110

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.