Browse FAQs

Preventa XCS - Are the XCSDMP7* or XCSDMPC7* or XCSDMR7* magnetic switches compatible to the XPSUAF safety relay

Published date: 23 September 2019

The XCSDMP7* or XCSDMPC7* or XCSDMR7* magnetic switches are perfectly compatible to the XPSUAF safety relay. Please refer to the attached document showing the XCSDM references to associate and the wiring diagram of the complete solution. Note that the other model of magnetic switch having contacts NC+NO XCSDMP5* or XCSDMC5* or XCSDMR5* can be monitored by the XPSUAF unit, in function selector position 3; corresponding diagram is shown in the XPSUAF user manual

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.