{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does Somachine support the Generic Windows PC target type?
Issue:
Unable to find the Generic Windows PC series as a target type in Vijeo Designer when launched via SoMachine.

Product Line:
SoMachine (all versions), Vijeo Designer (all versions)

Resolution:
SoMachine currently does not have the ability to use the Generic Windows PC Series as a target type. In order to use the Generic Windows PC target type, the standalone version of Vijeo Designer needs to be installed, registered, and have the unlock code entered to add the Generic Windows PC target type. The unlock code to use in the Standalone version is: VJDHTGTSPV62M

Schneider Electric Global