Browse FAQs

Can I use external 24V to connect on the STO input on the ATV320 drive?

Published date: 22 October 2019

Issue:
Can I wire an external 24V signal to the STO input on the ATV320 drive?

Product Line: 
ATV320

Environment:
All model numbers, all serial numbers

Cause:
Customer wanted to wire his own external 24V circuit to the STO input on the drive.

Resolution:
Yes, as long as the common of the 24V external signal tie to the common on the drive.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.