Browse FAQs

What is the parameter FNOD on the ATV212 drive?

Published date: 22 October 2019

Issue:
What is parameter FNOD being used on the ATV212 drive?

Product Line:
ATV212

Environment:
All serial numbers

Cause:
N/A

Resolution:
FNOD determines the source of the drive's speed reference when the drive is in remote mode.  The drive needs to be stopped to make changes to parameter FNOD.  Below is the source of the drive's speed reference:

1 is reference source VIA
2 is reference source VIB
3 is HMI or Graphic Display option
4 is Serial communication
5 is +/- speed

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.