Browse FAQs

Best methods to Improve Window's Server Performance?

Published date: 05 December 2019

Product Line
PME 7.x, PME 8.x, PME 9.0, Windows Server 2008, 2012, 2016

Environment
Windows Server Performance Issues
Cause
Server Performance Issues

Resolution

Best methods to improve Windows Server Performance

1. Change the pagefile settings.

By default, Windows creates a pagefile that it treats as virtual memory. Because Windows uses this file frequently, it's best to change the pagefile settings based on your system's needs and requirements. Doing so ensures that Windows will not have to wait on another application to finish using the hard disk before it can read data from the pagefile. 
For more information, please review FA384516

2. Keep your hard disks defragmented

Schedule set dates for the drive to be automatically defragmented

3. Use the NTFS file system

Although NTFS is the default file system for Windows servers, Windows does support the use of FAT and FAT-32 file systems.

4. Remove seldom-used utilities

Running an application you're not actually using is a waste of server resources.

5. Disable unused services

By disabling unnecessary services, you are shrinking the size of the executing code base, thereby reducing the chances of the server containing an exploitable security hole.

6. Log off

This is another example of a situation in which you can increase security and performance at the same time. You should always log off of a server when you're not actively using the console.

7. Adjust the server response

A server is different from a desktop computer in that applications are not usually run from the server's console. That being the case, it's best to optimize the server so that applications running in the background take priority.

You can do this by opening the Server's Control Panel and double-clicking the System icon. When Windows opens the System Properties sheet, go to the Advanced tab and click the Settings button found in the Performance section. Windows will now open the Performance Options properties sheet. Go to the properties sheet's Advanced tab and make sure that Windows is set to provide the best performance to background services.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.