Browse FAQs

What is the input voltage range for the BMXDAI1604?

Published date: 21 May 2020

Issue
The module is specified as 100... 120VAC, is the the full range?

Product line
Modicon X80 IO

Resolution
The specified sensor operating range for the BMXDAI1604 module is 85... 132V. 

The input ON is at >= 74V, 2.5MA
The input OFF is at <= 20V, 1mA

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.