{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What size are the cable ports on the NetShelter CX, and how many are there?
Issue:
Cables need to enter and exit the cabinet.

Product Line:
NetShelter CX2

Environment:
All versions and serial ranges.

Cause:
Knowing the dimension of the cable port allows a person to calculate how many cables can fit through the opening.

Resolution:

AR4000MV: two ports, 30mm x 95mm at the botton and 26mm x 68mm at the top.

AR4018A/AR4018IA: one port, 350mm x 120mm at the bottom.

AR4024A/AR4024IA: one port, 350mm x 120mm at the bottom.
AR4038A/AR4038IA: two ports, 350mm x 120mm, one at the top and one at the bottom.

Schneider Electric Global