Browse FAQs

What are the technical details of the integrated optical transceiver of TCSESPU093F2CU0?

Published date: 23 April 2020

Issue
The TCSESPU093F2CU0 has two Multimode ports (type 50/125) and this FAQ gives the technical details of the integrated optical transceiver. 

Product Line
ConneXium Switch

Environment
TCSESPU093F2CU0

Resolution
The TCSESPU093F2CU0 integrated optical transceiver has:
  • Maximum optical power: -14dBm
  • Transmit power: -23.5dBm
  • Receiver sensitivity: -31dBm
  • Loss budget: 7.5dBm 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.