Browse FAQs

What is the replacement for the XBTF024110 Magelis HMI?

Published date: 31 October 2019

Issue: 
Replacement model for the XBT-F024 series Magelis HMI (XBTF024110, XBTF024310, and XBTF024510)


Product Line:
Vijeo Designer, XBTF, XBTL1000, HMIGK


Resolution:
The replacement for the XBT-F024 model series HMI (including part numbers XBTF024110, XBTF024310 and XBTF024510) is the 
HMIGK5310. The HMIGK5310 is programmed using Vijeo Designer V6.2 development software. The XBTF project must be converted to Vijeo Designer either manually or via the Schneider Electric service group for a fee.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.