Browse FAQs

When using a VW3A3320 Ethernet IP option card in an ATV61 or ATV71, what do the status LED's indicate?

Published date: 28 October 2019

Issue:
What do the signaling LED's indicate when using a VW3A3320 Ethernet IP card?

Product Line:
Altivar 61, Altivar 71, VW3A3320

Environment:
All

Cause:
Documentation of status LED indications

Resolution:
Please refer to the attached file, which is page 30 of the ATV61/71 ModbusTCP manual - VW3A3320.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.