Can I start and stop the soft starter ATS22 30 times within 2 minutes time frame?
Published date:
22 October 2019
Issue:
Is it possible to start and stop the soft starter ATS22 30 times within 2 minutes time frame?
Product Line:
ATS22
Environment:
All serial numbers
Cause:
Customer needed to start and stop the soft starter that many times because of their applications.
Resolution:
It is not recommended to start and stop the soft starter ATS22 that many times. Too many starting and stopping of an ATS22 in a short time period can cause over heating issues.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.