Browse FAQs

What's the difference between the Magelis HMIBMOMA55DD1101 and the HMIBMOMA5DDF10L ?

Published date: 20 September 2019

Issue
The Magelis Box PC Optimized models HMIBMOMA55DD1101 and HMIBMOMA5DDF10L  are very similar in technical specifications. What is the difference between the two?

Product Line
Magelis Box PC Optimized (HMIBMO)

Environment
Physical HMI Characteristics

Resolution
The HMIBMOMA5DD1101 only has an 80GB M.2 SSD with no expandable slot.
The HMIBMOMA5DDF10L has comes with a 250GB M.2 SSD for storage with an additional 2.5" HDD/SSD slot, and because of that has a wider mounting profile.
Both models have 4GB DD3 RAM that is not expandable.

Please refer to the "Magelis Industrial PC, Edge Box and Display catalog" for more details on the HMIBMO lineup:
https://www.se.com/ww/en/download/document/DIA5ED2140501EN/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.