PME 9.0 numeric objects scaled in Vista are not scaled on Web Applications
Published date:
26 September 2019
Issue
In PME 9.0, when scaling numeric object values in Vista using units starting with "G", "M", or "K", the value is scaled in Vista but not when the diagram is viewed in the Web Applications Diagrams tab.
Product Line
Power Monitoring Expert 9.0
Environment
Web Applications
Resolution
Apply the latest PME 9.0 Cumulative Update (CU), which can be downloaded at FA368565.
Note: This was corrected in PME 9.0 CU1.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.