Browse FAQs

Do the Altivar Process Drives come with a speed pot and Hand Off Auto?

Published date: 22 October 2019

Issue:
Are speed pot and Hand Off Auto come with the Altivar Process Drives?

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer wanted to use speed pot and Hand Off Auto as control option.

Resolution:
No, speed pot and Hand Off Auto are not come with the drive.  However, customer can select the enclosed drive ATV660 that has speed pot and Hand Off Auto as a control option.  Please see the ATV660 instruction bulletin in the link below for a comprehensive list of the options in the ATV660:

https://www.se.com/us/en/download/document/NHA91297/
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.