Browse FAQs

What is the different between parameters FNOD and FMOD on the ATV212 drive?

Published date: 22 October 2019

Issue:
Is there a different between the two parameters FNOD and FMOD on the ATV212 drive? 

Product Line:
ATV212

Environment:
All serial numbers

Cause:
Customer couldn't find the parameter FNOD on the external keypad VW3A1101.

Resolution:
When using the external keypad, the parameter is FMOD can be found on the keypad.  On the drive's integrate display, the parameter FMOD is showed as FNOD.  Both of them are the same as Frequency Mode Set.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.