Browse FAQs

What is the FBE fault code showing on the ATV320 display?

Published date: 22 October 2019

Issue:
ATV320 display shows the FBE fault code.

Producl Line:
ATV320

Environment:
All serial numbers

Cause:
Customer said drive displays FBE on screen.

Resolution:
FBE is an indication of function block detected error.  You can go to ConF -> FULL -> FBN -> NFB -> FbFT (FB Fault) in order to check on the function block error.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.