Browse FAQs

Can I turn off RSTP from the HMI on the ALtivar Process Drives connected to Ethernet IP network?

Published date: 22 October 2019

Issue:
Can RSTP to be turned off on the HMI on the Altrivar Process Drives connected to Ethernet IP network?

Product Line:
ATV630 ATV930

Environment:
All serial numbers

Cause:
Customer didn't want to hook up the laptop to the drive.

Resolution:
No, the RSTP function cannot be found on the HMI.  You have to use SoMove software to access to the RSTP function in order to disable it. 

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.