Browse FAQs

How to add a network heading in Proworx 32?

Published date: 08 November 2019

Issue:
How do you add a network heading in a Proworx 32 program?

Product Line:
Proworx 32 programming software.

Environment:
Proworx 32 372SPU78001PDEV

Cause:
Not able to edit or add in a network heading in a segment  in the network navigator.

Resolution:
To be able to add or change a network heading first open the project.
1. Open Logic
2. Make sure that you have the Network Navigator open (if not open right click in a open spot in logic right click and and put a check on Navigation Tree)
3. Open the segment that you want to add the network heading
4. You can now slide he bar down or drag your logic screen up to see the Network Heading
5. Type in your Network Header name save and build to add in.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.