{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the max current for the P24 external supply on the ATV340 drive?
Issue :
Maximum current of the P24 external supply.

Product Line :
Altivar Machines, Altivar 340

Environment :
All models and serial number

Cause :
N/A

Resolution :
The P24 terminal is only available on the Frame Size 4 and 5 drives, ATV340D30N4 to ATV340D75N4
Max current is 0.8 A
Tolerance is minimum 19VDC and maximum 30VDC

Information is listed from the ATV340 Installation Manual NVE61069

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.