{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which connectors can be used for the BMXART0814
Issue
What are the options for wiring the BMXART0814 module?

Product line
Modicon X80

Resolution
There are two options:
  • BMXFCW301S (3m long) or BMXFCW501S (5m long) - One 40 pin FCN connector with color-coded flying leads, two required for BMXART0814.
  • BMXFCA152 1.5m or BMXFCA302  3m or BMXFCA502 5m cable plus ABE7CPA412 sub-base. Two sets required for a BMXART0814.

    ***The TELEFAST2  ABE-7CPA412 facilitates connection and provides a cold junction compensation device***

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global