Browse FAQs

How to update Symbol Link in EOTE V3.1

Published date: 14 October 2019

1. Issue
One customer uses Symbol Link to import variables taken from .smbp file (Machine Expert Basic) to EOTE. In case of the modification on the .smbp file, is it possible to make an update of this link inside EOTE?   
2. Environment
EOTE V3.1
3. Resolution
The answer is no. EOTE V3.1 does not support direct Symbol Link update. If you want to do an update, you need to delete the previous link first, then add the symbol link again. R&D team is considering improving this by supporting update symbol link feature in V3.2.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.