Browse FAQs

Access to SCADAPack Workbench\CAM ISaGRAF3 _Simul\ISA11 is denied

Published date: 20 October 2019

Access to Path 'C:\Program Files (x86)\Schneider Electric\SCADAPack Workbench\CAM ISaGRAF3\Simul\ISA11' is denied
SCADAPack Workbench 6 CAM3 may encounter Error During Simulation as below figure:
  • Platform:  SCADAPack Workbench 6 CAM3
  • Issue: While trying to run the same program in simulation mode and I get the following message:
                            'Access to Path 'C:\Program Files (x86)\Schneider Electric\SCADAPack Workbench\CAM ISaGRAF3\Simul\ISA11' is denied'

                                                          


Resolution:
  1. Go to the below path
                            C:\Program Files (x86)\Schneider Electric\SCADAPack Workbench\CAM ISaGRAF 3
  1. Right Click at 'Simul' folder > Properties >Security > and check if the current windows user has full control, if not please give the user full control by select the User >Edit > Full control >Allow


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.