Browse FAQs

Does the SA26PS and SA26PSR Switchboard Pull Section meet the EUSERC requirements for Access Opening or Conduit Entry

Published date: 22 October 2019

 Based on the EUSERC standard Drawings 327 Rev.3 Dated 10/08 and Drawing 345 Rev.8 Dated 10/08. The Access Opening requirement for 400-800 Amp Pull Sections is 24 inches Wide. The SA26PS and SA26PSR have an Opening A cess of 24 inches Wide as measured from the Interior Side Frames. The Overall Width of these sections is 26 inches. The Access Opening requirements should not be confused with the Conduit Entry opening. Currently the Conduit Entry opening for these Pull Sections is 22.41 inches wide. The EUSERC standard drawings refers to A cess Opening and not Conduit Entry. Please Note that EUSERC is US standard intended for Utilities.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.