Browse FAQs

Why I can't run in reverse in SoMove control panel?

Published date: 23 October 2019

Issue:
Drive will not run in reverse in SoMove when clicked on reverse in control panel.

Product Line:
ATV630

Environment:
All model numbers

Cause:
Customer can run drive in forward but not in reverse in SoMove control panel.

Resolution:
A correction request had been submitted to correct in the further version of ATV630 DTM.  For now, need to assign RRS = LIX  ( RRS = LI6 for example).  Then you will be able to use Reverse button in SoMove control panel to command drive to run in reverse.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.