Browse FAQs

How to read the speed reference on ATV71 drive using Ethernet IP 103/104?

Published date: 23 October 2019

Issue:
Why I couldn't read speed reference on ATV71 drive with Ethernet IP communication?

Product Line:
ATV71

Environment:
All model numbers

Cause:
Customer wanted to read speed reference on the ATV71 drive using Ethernet IP.

Resolution:
In somove, there is no access to rpm.  However, you can change it from the webserver.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.