Browse FAQs

How to clear the SD Card Error on the BMXNOE0100?

Published date: 24 October 2019

Issue:
I'm seeing the SD Card Error LED on solid on the BMXNOE0100. How can I clear this error?

Product Line:
M340

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
The likely cause of the SD Card Error was that the card was removed or inserted when the rack was powered up.
This error can be cleared by power cycing the rack or simply removing the BMXNOE0100 from the rack and reseating it into its rack positon.
In both cases, it will power up and get its configuration from the CPU module.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.