Browse FAQs

Why is there a shadow line on the Trend Graph in EcoStruxure Operator Terminal Expert?

Published date: 25 October 2019

Issue:
When using the Trend Graph in EcoStruxure Operator Terminal Expert, there is a secondary trend that seems to be a shadow of the real time trend data points that is a few seconds behind.

Product Line:
EcoStruxure Operator Terminal Expert V3.1 or higher

Resolution:
When the setting "Display Historical Data" is enabled in the Trend Graph properties in EcoStruxure Operator Terminal Expert, there will be a second plot on the graph showing the data stored as historical data. This second plot will appear in a lighter shade of the color used for the real time trend. To turn off this Historical Trend Graph, uncheck the check box "Display Historical Data" in the Trend Graph properties.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.