Browse FAQs

Where can I find the TM171ADMI USB Driver?

Published date: 29 October 2019

Issue:
Where can I find the TM171ADMI USB Driver for the M171/172 HVAC controller?

Product Line:
M172 HVAC controller

Environment:
Ecostruxure Machine Expert HVAC

Cause:
Looking for the download for the TM171ADMI driver for the TM172 controller.

Resolution:
The driver is installed with the software and the default install will place the driver executable in the following location,
C: Program Files(x86)/Schneider Electric/EcostruxureMachineExpertHVAC/Driver/USB-CDC
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.