Browse FAQs

What do the ATV61/71 2.1- 2.5 Signaling LED's indicate when a VW3A3310D option card is installed?

Published date: 31 October 2019

Issue:
What do the status LED's indicate?

Product Line:
Altivar 61, Altivar 71

Environment:
All

Cause:
Maintenance and troubleshooting

Resolution:
The 2.1- 2.5 signaling LED's indicate the status of a network connection. See attachment for details on each LED. 

You can also find full details about the VW3A3310D option card including installation, configuration, and troubleshooting in the ATV61/71 Modbus TCP/IP manual - Daisy Chain Ethernet card - VW3A3310D.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.