Browse FAQs

How do you set the two wire type to level control on the ATV600 Process drives?

Published date: 04 November 2019

Issue:
Two wire type to level control on the ATV600 Process drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All 

Cause:
Set two wire type to level to start on power up with start command

Resolution:
Programming example to set up 2 wire for level control.
Main Menu
Complete Settings
Command and References menu
Set 2-Wire type setting to LEL or Level 
Done

ATV600 programming manual 
https://www.se.com/ww/en/download/document/EAV64318/
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.