How to fix the error of Unsolved External Symbol ‘max’ & ‘min’ after UMAC
Issue
After converting the program by UMAC3.15, customer fail to build the program with IEC_BMDI_Q block in Control Expert, and reports the error information as bellow: Linker – Unresolved External Symbol: “max” Linker – Unresolved External Symbol: “min”
Product Line
Control Expert V14.0, UMAC 3.15
Environment
Control Expert V14.0, Win10 64Bit SP1
Resolution
Please install the “UMACLibInstaller.exe” from the attached for installing the UMAC library into the Control Expert V14.0. Then open the application and build to check whether the error has been fixed.
Released for:Schneider Electric Global
Attachment(s)
Unresolved External Symbol.png [129.12 KB]
UMACLibInstaller.exe [361.08 KB]
Explore more
Range:
EcoStruxure Control Expert (Unity Pro)
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.