{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
how to create a Web Dsigner application for the BMENOC0311 Factorycast module.
Issue
The purpose of this video is to demonstrate how to create a Web Dsigner application for the BMENOC0311 Factorycast module. The video also demonsstrate how create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familar with using both Unity and Web Designer.

Product Line
BMENOC0311

Environment
Windows 10

Resolution
The purpose of this video is to demonstrate how to create a Web Dsigner application for the BMENOC0311 Factorycast module. The video also demonsstrate how create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familar with using both Unity and Web Designer.

Schneider Electric Global