{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What purpose does the fuse of BMXDDI3202 and BMXDDI6402 serve or protect?
  1. Issue

What purpose does the fuse of BMXDDI3202 and BMXDDI6402 serve or protect? and is the information in User manual just an illustration or a mandatory requirement?

  1. Product Line
X80 IO module
  1. Environment
BMXDDI3202, BMXDDI6402
  1. Resolution
This fuse protects both the module and customer power supply. It protects the DDI module when there’s over voltage applied to module. And it protects the sensor power supply in case of the happening of short circuit malfunction inside the module. Since that it’s strongly recommended to apply this fuse.

Schneider Electric Global