{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can you put a breaker alone without fuses on the line side of the Altivar ATV16 unit or do you need both in series?
Issue:
Wondering if you can you put a breaker alone without fuses on the line side of the Altivar ATV16 unit or do you need both in series?

Product Line:
ATV16

Environment:
All

Cause:
N/A

Resolution:
We do not recommend that a circuit breaker be used without the fuses. The units have been tested and coordinated, with the fuses, we recommend. The circuit breaker alone may not adequately protect the unit.


Schneider Electric Global