{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why using SEL bloc with EcoStruxure Control Expert V15.0 (and lower) on BMEP586040 or BMEH586040 M580 PLCs lead to an exception (error code %SW124 = 0xEC10 on CPU) ?
Issue :
If  "SEL" bloc is executed with an input parameter with a size of 2 or 4 bytes and using it on a BMEx586040x M580 PLC, the CPU will go in exception with error code %SW124=0xEC10  because of a alignment problem in the optimized code of the bloc function "SEL".
Example Sell

Product line :
EcoStruxure Control Expert software tool with version V15.0 or lower.

Environment :
BMEx586040  with x= P or H
BMEH586040S

Resolution :
The issue will be fixed in a next revision of  EcoStruxure Control Expert (> V15.0)


Workaround :
Two easy workaround exist :

1 : Duplicate the SEL bloc as shown below (size not equal to 2 or 4 bytes anymore) :
Example Sell 2

2 : Use conditional MOVE bloc instead of SEL as shown below :
Example Move

Schneider Electric Global

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: