{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum altitude can TeSys Giga contactors be used without derating ?
TeSys Giga contactors can be used up to 5000 meters, and 3000 meters without any derating.

The derating table on MKTED210011EN for TeSys control contactors is also applicable for the TeSys Giga offer.

image.png

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.