{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to set IP address of a HMIGTO target when using Modbus USB Equipment connection in VJD 6.2 SP11?

In Vijeo Designer 6.2 SP11, we can't set HMIGTO IP address in the same network segment with a M340/M580 PLC when you try to connect the HMIGTO to the M340/M580 PLC via USB. As we know, the default IP address for M340/M580 PLC is 90.0.0.1, which we can't change. So we can't set the HMIGTO IP address as 90.0.0.XXX. Otherwise there will be no connection.

Schneider Electric Global