{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why do I get the error "Can't delete Type. It may be in use or all the types may not be analyzed." when I try to delete a DFB in EcoStruxure Control Expert?
Issue:
"Can't delete Type. It may be in use or all the types may not be analyzed." error when deleting a DFB


Product Line:
EcoStruxure Control Expert


Resolution:
The error below occur when there are function block instances that have not been deleted

image


Before deleting the DFB all function block instances must first be deleted
image

Schneider Electric Global