{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric corporate Website

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais

VIP300 manual

The VIP300 is a basic protection relay device. Here is its user manual:

What is the programming software for the Modicon M340, BMXP34xxxx?

Issue: What is the programming software for the Modicon M340, BMXP34xxxx? Product Line: Modicon M340, BMXP340xxxx,EcoStruxure Control Expert (Formerly Unity Pro) Environment: Cause: Resolution: The Modicon M340 is programmed with EcoStruxure Control Expert (Unity Pro). The lowest package you can...

What is the difference between isolated and non-isolated coaxial sockets? e.g. GUE7011W

A non-isolated coax socket is a standard socket. If you wish to install a socket to connect your TV coax lead into, this is what is required. Also, this version must be used for satellite installation as a two way signal is required. The satellite box does not only receive a signal, it also...

Will TwidoSuite software run on a Windows 10 machine?

Issue: Can TwidoSuite run on Windows 10 ? Product Line: Twido, TwidoSuite Environment: TwidoSuite Cause: Can't get Twidosuite to run on Windows 10. Resolution: No. TwidoSuite, Twido is an obsolete product and has been replaced with the M221 and EcoStruxure Machine Exert Basic ( formally TwidoSuite)...

What software is used to program the M221?

Issue: What programming software is needed for the M221 controller? Product line: All M221 controllers Environment: EcoStruxure Machine Expert Basic ( formally SoMachine Basic) Cause: Can not fine the SoMachine Basic software for download. Resolution: The M221 controller uses the EcoStruxure...

SoMachine 4.3 - how to connect to a controller without forcing a download

There are three files that are are important to connect as equal or without forcing you to re-download a SoMachine 4.1 project. They are .bootinfo, .bootinfo_guids and .compileinfo. 1. These files are generated when you Login for the first time to the PLC and the boot application is created. 2....

Conzerv ELF3200 series Instruction Manual.

Product Line ELF 3259 ELF 3234 ELF 3234-3 Resolution This manual includes instructions for the ELF 3259, ELF 3234, and ELF 3234-3.

What software is needed to program the M238?

SoMachine software is used to program the M238 PLC. Currently the latest version of SoMachine is 4.1.

Popular Video FAQsPopular Videos

Learn more through our Generic Knowledge FAQsGeneral Knowledge

NEMA 5-15 receptacle description

Issue : Which terminal is which in a standard household outlet? Cause : Informational Resolution : The NEMA 5-15 receptacle is the most common electrical receptacle in the United States and Canada. It is a two-pole, three-wire grounding receptacle which is used for a maximum of 15A and 125V. The...

How accurate are the APC Environmental Monitoring products?

Issue How accurate are the APC Environmental Monitoring products? Product Line Security and Environmental Appliances AP9320 AP9340 AP9612TH AP9312TH Supported sensors Environment All serial numbers All firmware versions Cause General accuracy information for users with the aforementioned...

How to reboot the SmartConnect Network Interface

Issue: How to reboot the SmartConnect Network Interface Product Line: SmartConnect enable Smart-UPS Environment: Smart-UPS SMC, SMT, SCL with built-in SmartConnect network port Cause: Need to reboot for X reason or need to establish connectivity or re-establish connectivity with SmartConnect cloud...

Did APC purchase the AirFlow Company?

Issue: Did APC purchase the AirFlow Company? Product line: Airflow Environment: Data Center Cooling Cause: Resolution: APC purchased Airflow in 2000 and formed a Network Air Division under APC. The best place to start is to call into our technical support line to identify the parts needed....

ATV320 corner grounded or side grounded Delta system

Issue: Customer has a corner grounded or side grounded Delta Power system, wants to be sure the drive will work with it. Product Line: ATV312/ATV31 Altivar 312, Altivar 31, ATV320 Environment: All part numbers, all models Cause: n/a Resolution: Yes, the drives can operate on this type of power...

What are the Commercial and Government Entity (CAGE) codes for Schneider Electric (US only)?

Product Line Schneider Electric Products Resolution The CAGE codes for Schneider Electric/SQUARE D are listed below: CAGE Code Company Address 04429 SQUARE D CO LEEDS MFG PLANT 940 MOORE ST NE LEEDS, AL 35094 05684 SQUARE D CO MIDDLETOWN MFG PLANT 1500 S UNIVERSITY BLVD MIDDLETOWN, OH 45044 07442...