Can prefabricated data centers cut construction carbon?
- Suraj Manohar Desai, Mahesha Munanjanappa, Wendy Torell & Ray Lizotte
- 08 Oct 2026
- 4 min
Prefabricated power modules reduced construction-phase embodied carbon emissions by roughly 80% compared with traditional stick-built electrical rooms. That’s what a recent analysis of a representative 5 MW data center deployment by Schneider Electric revealed. The savings stem primarily from reduced concrete, steel, freight, and on-site construction activity. Even under a conservative 60-year scenario that assumes enclosure replacements every 20 years, prefabricated designs maintained a carbon advantage of more than 50%. How important are construction choices in sustainable data center development? Dive in to find out.
But a large share of a data center's carbon footprint is already fixed before the first server is installed. It is decided during construction. For operators building AI-ready capacity, efficiency and sustainability are no longer separate objectives, and the building itself is where both start.
A Schneider Electric Data Center Research & Strategy group white paper, Sustainability Benefits of Prefabricated Data Centers: Core and Shell Carbon Reduction, finds that the construction method used for a data center’s core and shell can substantially change its embodied carbon emissions.
In a representative 5 MW data center deployment, prefabricated construction reduced construction-phase embodied carbon by about 80% compared to a traditional stick-built electrical room.
The study compared a conventional electrical room with five prefabricated power modules providing the same 5 MW capacity. Both occupied about 4,500 square feet, allowing the analysis to focus on the impact of the construction method.
Prefabricated construction reduced embodied carbon by approximately 80% at deployment
This is when it is compared with a traditional, stick-built electrical room.
Reduced concrete and steel requirements were the primary drivers of carbon savings
This is particularly executed through smaller foundation requirements.
The carbon advantage persisted over time
Even assuming module enclosures are replaced every 20 years, cumulative embodied carbon remained more than 50% lower after 60 years.
Core and shell design decisions materially influence upfront emissions
This affects site preparation, construction activities, freight, and material usage.
Prefabrication may unlock broader sustainability benefits
This goes beyond construction, including rightsizing infrastructure, optimising system integration, and improving lifecycle management.
One of the central challenges highlighted in the paper is that construction-related emissions are fundamentally different from operational emissions. Operational energy consumption can be reduced over time through efficiency improvements. Construction emissions cannot.
Once concrete is poured, steel is erected, and materials are transported to site, those emissions are already embedded in the facility. They become part of the project's environmental ledger on day one.
The paper focuses specifically on these embodied emissions by comparing two approaches delivering the same functionality and capacity:
- A traditional stick-built electrical room
- Five prefabricated power modules supporting the same 5 MW deployment
The results were striking. The traditional approach generated approximately 1.16 kilotonnes of CO₂e, while the prefabricated deployment generated 0.24 kilotonnes of CO₂e.
To understand why the gap is so large, it helps to examine the four sources of carbon emissions associated with core and shell construction:
- Above-ground clearing
- Freight of materials
- Site construction activity
- Materials used
Traditional construction depends on extensive on-site activity. Excavation, foundation building, concrete pouring, steel installation, facade construction, roofing work, and interior finishing all require labor, equipment, fuel, temporary infrastructure, and repeated material deliveries.
Prefabricated Modular Data CenterTM changes that equation. Much of the work is completed in a factory before modules ever reach the site. Instead of constructing an entire building around equipment, the enclosure itself arrives largely complete and requires placement, connection, and limited finishing work.
Stick-built | Prefabricated | Reduction | |
| Action | |||
| Emissions contributions | |||
| Above ground clearing | 0.010 CO₂e | 0.010 CO₂e | 0% |
| Freight | 0.176 kt CO₂e | 0.028 kt CO₂e | 85% |
| Site construction | 0.149 kt CO₂e | 0.037 kt CO₂e | 75% |
| Materials | 0.823 kt CO₂e | 0.167 kt CO₂e | 80% |
Source: Schneider Electric
Sustainability gains are driven less by technology and more by materials. Concrete accounted for approximately 58% of total emissions in the stick-built scenario, making it the single largest contributor to embodied carbon. Freight represented 15%, site construction activities 13%, and structural steel 8%.
By reducing the need for large slab-on-grade foundations and extensive building structures, prefabricated designs require significantly less concrete and steel. Instead, they rely on localized support structures such as reinforced concrete pads and pilings sized specifically for the modules.
A common question surrounding prefabricated infrastructure concerns longevity. If modules need replacement sooner than traditional structures, could long-term emissions offset the initial savings?
Researchers used a deliberately conservative scenario, where module enclosures would be replaced every 20 years while the traditional electrical room remained in service for a full 60-year period, and where future replacement modules would deliver no manufacturing or decarbonization improvements.
Even under those assumptions, the carbon advantage of prefabricated modules remained substantial. In fact, even after accounting for two full module replacements over a 60-year horizon, prefabricated electrical rooms still delivered lower cumulative embodied carbon than their traditional counterpart.
The analysis showed that the initial carbon savings were large enough to outweigh the impacts of future replacements, preserving a meaningful lifecycle advantage.
The findings suggest that sustainability assessments should begin earlier in the design process than many organizations currently assume.
As AI drives another wave of global data center expansion, placing increasing pressure on energy and resources, infrastructure efficiency and resilience become strategic imperatives. Therefore, if two facilities deliver the same capacity and functionality, the wisest strategy is to avoid locking in the higher carbon burden before the first watt of IT load is ever switched on.
Want to explore the findings in greater depth? Download the Schneider Electric white paper, "Sustainability Benefits of Prefabricated Data Centers: Core and Shell Carbon Reduction", for a detailed analysis of embodied carbon impacts, lifecycle assumptions, methodology, and practical guidance on how prefabricated designs can support more sustainable data center development.

Latest in Data Center Research & Strategy
Exploring DCIM and EcoStruxure IT solutions
Generative AI inferencing ramp-up
The price of invisible downtime
800VDC: Powering the future of AI data centers
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.