Skip to main content

Are you ready to become energy efficient, sustainable, and profitable?

We’re passionate about helping other companies achieve their profitability and sustainability targets through energy management and automation.

In my view there are three essential things to consider:

  • · Energy consumption

  • · Sustainability

  • · Productivity & profitability

In the past these three elements were incompatible – an either/or situation. It was enough for a business to be profitable. These days productivity can’t be separated from energy efficiency and sustainability. Industry has shifted to eco-efficiency. To attract investment, talent, and customers, you must show real commitment to climate change action and sustainability as well as profitability. Without this it will become harder to remain competitive. And finally, embracing sustainability and energy efficiency must and does ultimately lead to higher productivity and profitability.

Eco-efficiency starts with measurement

The right level of measurement and visibility is key. The only way industrial businesses can do energy efficiency, profitability, and sustainability effectively or better than everyone else is by acting on insights from process and business system data in real time. It’s essential to see each of these three things as a production variable which can be measured and eventually managed in real time using the latest in IIoT technology.

Read more on the challenges of accurate measurement in this blog:

https://blog.se.com/sustainability/2021/04/29/are-you-ready-to-become-energy-efficient-sustainable-and-even-more-profitable-now/