Opinion Piece: Moore's law, sustainability and data centres: How software will handle the future data explosion
The data centre sector’s proven record of dealing with massive demand growth can be applied to wider sustainability challenges
The data centre sector’s proven record of dealing with massive demand growth can be applied to wider sustainability challenges
By Natalya Makarochkina - Senior Vice President, Secure Power Division, International Operations, Schneider Electric
An important principle in the development of IT over the decades has been Moore’s Law. Simply put, it predicted that transistor density in processors would double every two years as development progresses.
Despite many predictions of its demise, it has remained a more or less guiding principle. However, what is perhaps less well known is a similarly persistent trend in the data centre space.
Despite a six-fold increase in the data being processed since 2010, data centre energy consumption has only risen by 6% to 2018 (Masanet et al, 2020). How has that been possible, and how does it inform sustainability developments into the future?
Where does the data come from?
To contextualise this development, we must first understand where the data processing increase has come from.
The Apple iPad got its debut in 2010, which also saw the introduction of Instagram and Microsoft’s Azure cloud service. 2011 introduced us to Minecraft, Snapchat, and Uber, with 2013 bringing Amazon’s Alexa, accompanied by Xbox One and PlayStation. 2017 brought Fortnite and Tiktok.
Social media engagement over the period increased manifold, while global data production went from estimates of 2 zettabytes in 2010 to 41 zettabytes in 2019. IDC estimates global data load will rise to a staggering 175 zettabytes by 2025.
The pandemic effect has been substantial, with the MENA region seeing a big increase in messaging and social media usage: Social Media Users in MEA and Latin America spend the most time on social networks, averaging over 3.5 hours a day.
More than half of users in MEA (57%) reported (May 2020) spending even more time on social media as a result of the pandemic. Similarly, in a separate study, 71% of Middle East respondents reported WhatsApp and other messaging apps usage increased since the outbreak of the pandemic.
What impact does all that data have?
To understand the impact of this data explosion, a concept has been developed called data gravity. Coined by engineer David McRory, the term refers to the tendency of an accumulation of data to attract applications and services toward it, precipitating further accumulation, which can lead to immobilisation of the data, as well as underutilisation. Data that grows too big, too fast can become immobile, reducing its value and increasing its opacity. Only low latency, high bandwidth services, combined with new data architectures can combat this growing, and largely undocumented phenomenon.
What tech developments have made this possible?
Multiple technological developments can account for this data explosion being handled with only minimal increases in energy consumption, from improvements in processor design and manufacture, through power supply units and storage, but also the migration of workloads from on-premises infrastructure to the cloud.
Schneider Electric has been committed to sustainable business for decades. That has meant a renewed focus on efficiency in all aspects of design and operation. Gains have been made in efficiency in power and cooling, with UPS systems and modular power supplies showing significant gains with each generation, culminating in the likes of the current Galaxy VL line. This line’s use of lithium-ion batteries has not only increased efficiency, it has extended operational life, reduced environmental impact in reducing raw materials, and facilitated “energized swapping”, where the addition and/or replacement of power modules can be performed with zero downtime, while increasing protection to operators and service personnel.
Advances in cooling, such as flow control through rack, row and pod containment systems, liquid cooling, and intelligent software control ensure that the pure data processing gains are met and matched.
By ensuring that every link in the chain of power from energy grid to rack is as efficient, intelligent, and instrumented as possible, we provide the right basis for the rapid development in compute, network, and storage that continues daily.
Where does software and apps fit here?
Another key element of the technological development that has allowed such relentless efficiency has been the application of better instrumentation, data gathering, and analysis that allows for better control and orchestration. This was illustrated by Google’s DeepMind AI, where the energy used for cooling was reduced at one of its data centres by some 40% in 2016, which represented a 15% overall reduction in power usage.
This was accomplished using historical data from data centre sensors such as temperature, power, pump speeds, setpoints, etc, to improve data centre energy efficiency. The AI system predicted the future temperature and pressure of the data centre over the coming hour and made recommendations to control consumption appropriately.
The development of data centre infrastructure management (DCIM) systems has continued apace too, allowing the integration of AI to take advantage of all of these hardware and infrastructure developments. These experiments are now features, allowing unprecedented visibility and control. For those designing for new developments, software such as ETAP, allows power efficiency to be built into the design from the outset, while also accommodating microgrid architectures.
What new data sources will contribute to this?
The data explosion is expected to continue increasing, with developments such as industrial IoT, 5G, with increasing general automation and autonomous vehicles as driving factors. The data that will be generated, far from the centralized data infrastructure, must be handled, processed and turned into intelligence quickly, where it is needed.
New data architectures are expected to improve efficiency in how all of that is handled. Edge computing is seen as an important approach to manage more data being generated at the edge.
In one example, genomic research generates terabytes of data, often daily. Sending all that data to a centralized data centre would be slow, demand high bandwidth and be inefficient. The Wellcome Sanger Institute created an edge computing approach that allowed it to process data close to where it is produced, the genomic sequencers, with only what is necessary centralized. This saves on storage, bandwidth and speeds the time to intelligence from data. That is where the edge paradigm has come to us, said Simon Binley, data centre manager, Sanger Institute.
Modular data centres, micro data centres and better storage management will all contribute to handling this developing wave efficiently, keeping that data centre energy consumption line as flat into the future. In the MENA region, 5G, and
centralisation with edge architectures will be balanced by more hyperscale facilities linking major demand centres.
What effects will this have on the whole data ecosystem?
However, efficiency must extend through not just the supply chain, but also throughout lifecycles. Vendors, suppliers, and partners must all be engaged to ensure that no part of the ecosystem lags in applying the tools to ensure efficiency. This applies as much in the design time of new equipment and applications as it does through working life and decommissioning. Understanding how an entire business ecosystem impacts the environment will be vital to truly achieving net zero goals.
Agreed standards, transparency and measurability are all vital factors to ensure results.
These considerations are taking hold across the region, great efforts being made to do better. Greater transparency is now accepted and embraced, with more and more organisations reporting their progress.
Tools and processes shared
The data centre sector has much that will be of use to organisations and industries going on the journey of sustainability towards increasing circularity. With the expertise and experience in efficiency, combined with the tools and intelligence from operations, and deep commitments to tight targets for net-zero operations, the data centre sector can not only handle the data explosion and digital demands of the world, but do so sustainably, while providing others with the tools and insights to do the same for their respective sectors.
For further reference, see our Cloud and Service Provider page, with data centres of the future views here.
Attached files
Opinion Piece- Moore's law, sustainability and data centres- How software will handle the future data explosion .pdf
PDF, document02/12/2022View asset
Contact press

Schneider Electric Sub-Saharan Africa Media Relations
0112546000 africa.pr@se.com
Adoption of Wiztrust's Blockchain Certification Platform
From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.