Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.

Optimizing Buildings for Low-Occupancy

By Marwan Zeidan, Real Estate and Healthcare Segment Director, Middle East and Africa, Schneider Electric

Building managers can optimize systems to achieve the most efficiency in times of low-occupancy 

The COVID-19 pandemic has led to thousands of empty buildings, as offices, malls and other commercial spaces have shut down across the MENA region. Even as some facilities, including malls, begin to reopen, they are operating at drastically reduced occupancy and are likely to do so for some time yet. In the UAE, all malls must maintain an occupancy ceiling of 30 percent of the mall, retail outlet or restaurant’s common and gross leasable area.

Many other buildings, including hotels and offices, are not likely to return to normal operations for a considerable length of time. Occupancy levels in Dubai’s hotels dropped by almost 30 percent year-on-year for the first week of March amid coronavirus concerns, according to data and analytics company STR. For building managers, facilities managers, owners and operators, having buildings at low or zero occupancy for extended periods of time, means a significant change in operating requirements, and a need to adjust building systems accordingly.

To secure a successful restart, now is the time to plan for operational optimization, to validate your property's business model and to adjust the operating concept for long-term value creation potential. From repurposing a property to adapting new strategies and approaches to secure a strong comeback for your business assets once the industry restarts, UAE stakeholders are considering a multitude of things from operational changes to strict hygiene measures in line with the government’s efforts.

The process of switching to low occupancy operations should start with a checklist of all your major HVAC and building automation assets, including chillers, air handlers, boilers, fan coils, packaged terminal air conditioners, and rooftop units. You need to know which of these key components are in operation, drawing energy and managing environmental conditions.

Critical First Steps

Before you get started on making adjustments to systems, it’s very important to document any changes that are made to systems and parameters. The typical low-occupancy set points that are used during weekends can be exceeded when facilities are unoccupied for months, so setpoints for temperature can move more drastically.

You should also factor in the changes to BTU load. HVAC systems are calibrated to a certain estimated BTU load for typical occupancy, but that will change with low occupancy.

Take advantage of variable speed drives (VSDs). Your building’s systems are designed for near full capacity, not low capacity. With a fixed speed drive, your energy use will remain constant regardless of output.

Any reduced-occupancy plan also needs to allow for remaining staff, so you should consider the essential areas that they still need to occupy and ensure staff are still going to be comfortable.

During low occupancy, venting out particulates and maintaining proper carbon dioxide dilution is still necessary. Overall, the idea is to ease off temperature controls to boost energy efficiency. You can consult your building automation service partner for optimal settings.

Humidity stills needs to be monitored, as mold and moisture can become a problem if indoor dew points are not properly maintained.

For IT systems, it is important to maintain the pre-defined setpoints for temperature to prevent any overheating. Most electrical rooms, however, are actually rated for outdoor operations, meaning higher temperatures can be safely maintained, which can be another source of energy saving.

Commercial kitchens and similar areas, which have equipment including exhaust fans and make-up fans, should be focus areas. Fans, freezers and refrigerators that are often set to run 24/7, can be shut down entirely if the kitchen facilities are not in operation.

Water systems should not be shut off, and it is important to make sure that you maintain minimum levels of water flow through the system. Stagnant water creates a health risk in domestic systems and can lead to higher than normal corrosion in non-potable systems. Boilers and hot water systems can be reduced or shut down, after taking specialist advice.

Finally, when making all these changes, it is important to monitor the building, and to keep documenting settings and processes. Regular monitoring of the facility will help to ensure that changes are not causing any problems such as moisture or hotspots, and to ensure that the changes are having the desired effect.

About Schneider Electric

At Schneider, we believe access to energy and digital is a basic human right. We empower all to make the most of their energy and resources, ensuring Life Is On everywhere, for everyone, at every moment. 

We provide energy and automation digital solutions for efficiency and sustainability. We combine world-leading energy technologies, real-time automation, software and services into integrated solutions for Homes, Buildings, Data Centers, Infrastructure and Industries. 

We are committed to unleash the infinite possibilities of an open, global, innovative community that is passionate about our Meaningful Purpose, Inclusive and Empowered values. 

For more information, go to www.se.com/za.

<!-- Start SmartBanner configuration --> <meta name="smartbanner:title" content="mySchneider"> <meta name="smartbanner:author" content="Schneider Electric SA"> <meta name="smartbanner:price" content="Free"> <meta name="smartbanner:price-suffix-apple" content=" - On the App Store"> <meta name="smartbanner:price-suffix-google" content=" - Google Play"> <meta name="smartbanner:icon-apple" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:icon-google" content="//lh3.googleusercontent.com/lAVirntKlp63vbntUZvOkMvZI8fE4rIoA5Lwif9M09VxzFhcWE21sTDYqJqOqIPqg4m4=w300-rw"> <meta name="smartbanner:button" content="VIEW"> <meta name="smartbanner:button-url-apple" content="http://m.onelink.me/e5bff3e5"> <meta name="smartbanner:button-url-google" content="https://app.appsflyer.com/com.schneider.qrcode.tocase?pid=Web&c=Smart_app_bannerZA"> <meta name="smartbanner:enabled-platforms" content="android"> <!-- End SmartBanner configuration --> <link rel="stylesheet" href="[PublicationUrl]/assets-re1/css/smartbanner.min.css" /> <script type="text/javascript" src="[PublicationUrl]/assets-re1/js/smartbanner.min.js"></script>