Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Choose another country or region

  • Schneider Electric introduces Easy UPS 3S to Africa

Johannesburg South Africa, 16 July 2018 - Schneider Electric

Schneider Electric South Africa, the leader in the digital transformation of energy management, automation and power protection, has announced the launch of their Easy UPS 3S in Africa.

Making business continuity easy for small and medium businesses, Easy UPS 3S is a 10-to-40kVA Uninterruptible Power Supply (UPS) that offers robust electrical specifications and compact design.

Easy to install, easy to use, and easy to service, the Easy UPS 3S is an exceptional combination of optimised footprint design and advanced product features, providing protection for critical equipment from damage due to power outages, surges and spikes.

The unit delivers up to 96% efficiency in double conversion mode and up to 99% efficiency in energy-saving ECO Mode, taking the industry standards for the 10-to-40kVA UPS to a new level.

Available with or without batteries, to address different business needs, Easy UPS 3S users also benefit from the start-up service option to ensure the unit is configured properly and safely for optimal performance, reliability, safety, and peace of mind.

Easy UPS 3S addresses a market need we have seen for a solution that offers best-in-class power availability, reliability, manageability, quality, and convenience for small and medium businesses, data centres, and manufacturing facilities,” says Riaan de Leeuw, Vice President, Schneider Electric ITD Anglophone Africa.

We look forward to bringing this new 3 phase 10-to-40kVA offer to the continent, where Easy UPS 3S is ideally suited for use in a wide range of industries and environments.

Rugged, with a wide input voltage window and strong overload protection, this new offer has been designed and tested following rigorous Schneider Electric procedures - making it an excellent fit in both the data centre space and in light industrial environments.

It rolls into position quickly and installation is straightforward. It features an intuitive display interface for easy configuration and monitoring, and customers can monitor and manage the UPS status remotely through Schneider Electric’s EcoStruxure™ IT cloud-based and on-premise software suites,” he explains.

In addition, Easy UPS 3S boasts short delivery time and wide variety of applications to make it easily adaptable for any small and medium business.

Schneider Electric South Africa’s global service setup, with strong, local networks of service specialists, provides our customers with a full range of services throughout the complete Easy UPS 3S life cycle,” concludes de Leeuw

Other innovative and user-friendly Easy UPS 3S features include:
  • Operating temperature up to 40ºC
  • Conformal coating for protection in rugged environments
  • Easy to replace dust filter
  • Easy service access via the magnetic front panel
  • Internal, external, and third-party battery options
  • Easy monitoring and management with EcoStruxure IT’s cloud-based and on premise software suites when you buy the optional Network Card.
  • Easy Loop test verifies UPS performance before you connect your load, without the need for a load bank

To learn more about Easy UPS 3S, please click here

About Schneider Electric
Schneider Electric is leading the digital transformation of energy management and automation in homes, buildings, data centres, infrastructure and industries. With global presence in over 100 countries, Schneider is the undisputable leader in Power Management – Medium Voltage, Low Voltage and Secure Power, and in Automation Systems. We provide integrated efficiency solutions, combining energy, automation and software. In our global Ecosystem, we collaborate with the largest partner, integrator and developer community on our open platform to deliver real-time control and operational efficiency. We believe that great people and partners make Schneider a great company and that our commitment to innovation, diversity and sustainability ensures that Life Is On everywhere, for everyone and at every moment.
For more information, go to https://www.se.com/za

See all Schneider Electric news

All news