Welcome to the Schneider Electric Website

Welcome to our website.

You can choose another country to view available products or go to our Global website for company information.

Choose another country or region

  • Schneider Electric releases new meter for energy cost management applications

Schneider Electric releases new meter for energy cost management applications

Commercial building managers, requiring energy cost management applications from their meters, can review the new EasyLogic PM2000 series from Schneider Electric.These are accurate and modular power and energy meters designed to provide all the essential electrical system measurements needed.

“Our customers, especially those that are sub-billing or allocating costs, are looking for accurate metering, more power quality information and to understand problem areas in order to fix them quickly,” says Nathan Potgieter, Offer Marketing Specialist, EcoBuilding, of Schneider Electric South Africa. “They also want data accuracy from their meters, so they can better understand the power served to customers in their facilities. We designed the PM2000 series to meet these specific needs.”

Ideally suited for energy cost management applications in commercial buildings, this series of meters have Accuracy Class 1.0 as per IEC 62053-21 and Class 0.5S for active energy test clause as per IEC 62053-22.

They also offer customisable rate counters, so users can choose to measure, for example, kgC02/kWh, or tariff rate based on energy consumption. They also provide reactive energy accuracy IEC 62053-24 Class 1.0 for increased precision, minimising errors and potential penalties that cost money. They allow simple integration within existing building management systems; the combined accuracy and I/O options make EasyLogic PM2000 meters ideal for even the most demanding environments.

The meters also ensure data security and integrity. The meters and their input signals are also protected from tampering with terminal covers. Field-configurable passwords prevent unauthorised changes and help avoid the resetting of stored data (energy, max demand, min/max). Users can even enable/disable the COM port to protect against possible misuse or cyberattack.

Engineered on a compact, modular and flexible platform, PM2000 series meters are field upgradeable, easy to install and set up, with standard terminal orientation (top & bottom) and 13 supported wiring configurations. They have the versatility to perform nearly any metering job at key points within a customer’s electrical system. Meters are available in both LED and LCD panel-mount form factors and boast high-visibility displays.

For more information, go to www.schneider-electric.co.za.

About Schneider Electric

Schneider Electric is the global specialist in energy management and automation. With revenues of ~€25 billion in FY2016, our 160,000+ employees serve customers in over 100 countries, helping them to manage their energy and process in ways that are safe, reliable, efficient and sustainable. From the simplest of switches to complex operational systems, our technology, software and services improve the way our customers manage and automate their operations. Our connected technologies reshape industries, transform cities and enrich lives. At Schneider Electric, we call this Life Is On.

www.schneider-electric.co.za

See all 2017 Press Release

All news