Product FAQs

Ask a Question

What is the default user name and password for programming the web pages on the ATV58 Ethernet option card?

Issue:
What is the default user name and password for programming the web pages on the ATV58 Ethernet option card?

Product Line:
Altivar 58

Environment:
All

Cause:
N/A

Resolution:
The default user name is :USER
The default password is: USER
Must be capitalized!
See the Altivar 58 Ethernet Modbus TCP/IP Communication Option VW3A58310U Instruction Guide for more assistance.
Was this helpful?
What can we do to improve the information ?