Product FAQs

Ask a Question

Using the StruxureWare DCE Linux internal browser to launch to devices causes an error when the DCE client is installed on some Linux systems.

Issue:

Using the StruxureWare DCE Linux internal browser to launch to devices causes an error when the DCE client is installed on some Linux systems.

Product Line:
StruxureWare Data Center Expert

Environment:

Linux
StruxureWare Data Center Expert version 7.x

Cause:

This issue is known to occur on some Linux systems when the internal browser is used to automatically log in to the web interface of devices that use basic authentication.

Resolution:

In the StruxureWare DCE client, uncheck the option to Use the Internal Web Browser when Launching to Devices in Browser Settings, accessed from the Client Preferences in the File menu.
Note: You must now manually log in to devices that use basic authentication.
 
Was this helpful?
What can we do to improve the information ?